Hi
I want to replace 2 AA batteries with 3.7v lithium batteries so I need a 3v converter suggest me some widely available Ic's.
optional:
Is there any 3.7v 600mah battery charger with inbuilt 3v converter ic's ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bharath,
Since this is battery powered, you may want to look at the TPS706. This is a very low ~1uA IQ LDO which could be great for powering the MCU (but it is limited to 150mA). When the device is enabled, then can can power either a higher current LDO or DC/DC to provide the higher current. The smallest size LDO we have at the moment for ~500mA is the TPS7A3701DRV.
Also, if you need a voltage monitor/reset IC, the TPS3831 is probably the lowest IQ device on the market. It comes in a 1x1 package (so smaller than a discreet RC) and its IQ is only 150nA!
Let me know what you think.