Dear all,
I'm developing 2s1p 1,500mAh Li-ion battery pack using BQ40Z50-R1 with 1-LED display.
LED is designed to light on 30% of the SOC.
To evaluate function of the LED, I adjusted the battery to 30% of the SOC with several charge and discharge.
note;battery voltage around 7.2V
Then LED lighted on correctly.
After that, I left the battery for long term at the state of [PRES] = 0.
After two week, I checked the battery LED but it was still light on though it may less than 30% of SOC.
note;battery voltage around 7.18V, current consumption is around 2mAh/day
Then, I tried to change the state of [PRES] = from 0 to 1. After that, LED is no longer light on.
To know value of the SOC, I confirmed the battery with bqstudio. As a result, certainly the SOC was 28%.
So I think remaining capacity can't update correctly at the state of [PRES] = 0.
How can I solve it?