This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do we have higher efficiency DCDC to upgrade LM25011?

Other Parts Discussed in Thread: LM25011

Hi team,

My customer is now finding light load DCDC part. LM25011 can meet almost all of their target including:

1. The adjust Constant current output;

2.  Power good;

3. Soft start function

4. Up to 1A output current and output voltage can cover 5V~9V with input voltage up to 24V;

But the only thing is that the LM25011's efficiency is low at light load, as the application is low power needed, so customer hope to realize high efficiency at light load, such as input 12V, output 5V/30mA, the efficiency can be up to 90%.

Do you have some good recommendation to replace LM25011? Thanks for the support!

Best regards,

Sulyn Zhang