Hello,
In my application, I do not want to recharge battery so i connected a super capacitor to VSTOR not VBAT. I made this VBAT pin floating because Buck, Boost & VOUT is monitored by VSTOR voltage threshold not VBAT.
Is it okay to connect a super capacitor to VSTOR as a storage element? System load is connected to VOUT pin.
Application requirements:
VOUT: 3V
VBAT_OV : 4.2V
Application is using VBAT_OK to turn on/off the system load connected to VOUT. What are the limitations to such a system? Please give me some suggestions.