Hi,
We are designing a power adapter module for lighting control system. We are using LM3404HV. The requirement is to drive LED Strips ( 36 numbers , 1W each LED) , voltage required is 52V to 62V @ 36W. Previously the LED strip was driven by the AC to DC Ballast. The power adapter module is designed to replace AC to DC Ballast. The Ballast DC output is 52V to 62V @ 36W. with Load.. With no Load the voltage can go upto 69V.
The query is Whether the LM3404HV be used to drive LED's with 36W Power, DC voltage of 52 to 62V and current 700mA to 1A max?
Currently the Input to the Power adapter module is from POE PSE switch which can supply IEEE802.3 af and at specification. Power upto 60W. A POE PD module is used on Board to convert the voltage from 48V to 24V.
The PD module output of 24V is Boosted to 64V using TI TPS40210 Boost regulator. The output of TPS40210 is used to input of LM3404HV. here boost and LED driverer is used in two chip solution for thermal consideration. TPS40210 does not support Thermal protection shutdown. Where as the LM3404HV has the Thermal shutdown feature.
Kindly let me know the maximum output power supported by LM3404HV.
Regards,
Sumathi