HI
I need to generate -5V (Negative 5V) @ 500mA or 300mA in smallest possible footprint.
The Input can be 12V or +5V.
Pls suggest proper solution.
Ragards,
Amit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.