This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC to DC step down switching regulator using LM5088MH-1/NOPB

Other Parts Discussed in Thread: CSD17579Q3A, LM5008

hi,

i have designed DC to DC step down switching regulator using LM5088MH-1/NOPB with input voltage range 9V to 22V and output voltage 5V,output current 10A.the schematic is generated from TI webench design and components are used as per the webench design. when i put load of 20% of output current ,that output voltage is droping to 4.5v with supply input of 9V and HG of the LM5008 is showing 0.8V ,actually it should be 1.5V minimum (VGS(th)) to drive the MOSFET (CSD17579Q3A) but it is not happening what could be the reason

2021.Doc1.pdf

  • Hi Prakash,

    The LM5008 is a non-isolated controller, I will move the post to the non-isolated forum and one of the apps engineer will answer your post.

    Regards

    Peter
  • hi,

    i have designed 

    Artifex Ghostscript 8.60 (2007-08-01)
    Copyright (C) 2007 Artifex Software, Inc.  All rights reserved.
    This software comes with NO WARRANTY: see the file PUBLIC for details.
    peelstring status: true: '% Copyright'
    peelstring status: true: '%!PS-Adobe-'
    Loading NimbusMonL-Regu font from %rom%lib/n022003l.pfb... 2495600 1176462 1871424 580208 1 done.
    %%[ ProductName: Artifex Ghostscript ]%%
    %%[Page: 1]%%
    %%[LastPage]%%
     ps2pdf -sDEVICE=pdfwrite -dNOPAUSE -dNOSAFER -dAutoRotatePages=/PageByPage -dPDFSETTINGS=/screen
     -dCompatibilityLevel=1.3 -sstdout=C:\Users\prakash\AppData\Local\Temp\g2tk4bpx -sOutputFile=C:\Users\prakash\AppData\Local\Temp\g2tk4bpx.iul
    
    ith input voltage range 9V to 22V and output voltage 5V,output current 10A.the schematic is generated from TI webench design and components are used as per the webench design. when i put load of 20% of output current ,that output voltage is droping to 4.5v with supply input of 9V and HG of the LM5008 is showing 0.8V ,actually it should be 1.5V minimum (VGS(th)) to drive the MOSFET (CSD17579Q3A) but it is not happening what could be the reason