Hi Sir,
May I know TPS65286 how calculate MAX Duty cycle? because we can't find Toff(min).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello..
Theoretically, it can get 100%, BUT there is limited condition. please refer to 8.2.9 in DS.
To improve drop out, the device is designed to operate at 100% duty cycle as long as the BST to LX terminal
voltage is greater than the BST-LX UVLO threshold which is typically 2.1 V. When the voltage between BST and
LX drops below the BST-LX UVLO threshold the high-side MOSFET is turned off and the low-side MOSFET is
turned on allowing the boot capacitor to be recharged.
Regards,
yuchang