This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24032A: STAT1 and STAT2 no stables.

Hi, I have designed one board with this IC, all is working well: battery charge, battery discharge, power supply the only thing that doesn't fit the product specification, is that, at the end of the battery charging process, with the battery voltage of 4.2V, Io(Bat) = 0 and V iset1 = 0 the voltages Vstat1 and Vstat2 are not stables and respectively high and low, but are both a square wave, with a small duty cycle.

What could be the problem or is it normal?

Thank.

Gianluca.