Hi TI members,
I was asked the following question from my customer.
Is there any method to disable OUTPUT except applying COMP pin to low?
He assumes VCC is applied in this case.
Best Regards,
Yaita / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI members,
I was asked the following question from my customer.
Is there any method to disable OUTPUT except applying COMP pin to low?
He assumes VCC is applied in this case.
Best Regards,
Yaita / Japan disty
Hello Yaita,
I reviewed the block diagram and there is a VREF good comparator. If you pull down on VREF this would shut down the device. However this short circuit current is 60 + mA so this is not advisable.
The other option is to force the device into UVLO by dropping or removing the VDD voltage.
I did review the data sheet and the comp pin is current limited to you can pull it down to ground to demand 0% duty cycle. The block diagram in figure 14 has this limited to 500uA. The data sheet give a 500 uA typical.
I know that your customer was looking for other options to shut down the gate drive; however, pulling down on the COMP pin is probably the best choice.
Regards,
Mike
Hi Mike-san,
I appreciate for your support!
>If you pull down on VREF this would shut down the device. However this short circuit current is 60 + mA so this is not advisable.
I understood I should see Figure 5.
Could you tell me threshold voltage of VREF good comparator as a reference?
In addition, Can I see the following datasheet for UC2845AQ?
http://www.tij.co.jp/jp/lit/ds/symlink/uc2845.pdf
I have seen the following datasheet until now.
http://www.tij.co.jp/jp/lit/ds/symlink/uc2845aq.pdf
Best Regards,
Yaita