Dear, All
I will ask about the BAT pin of BQ2057.
The absolute maximum rated value of BAT pin is written as "VCC + 0.3 V" on P5 of the data sheet.
However, this is inconsistent with the sentence of "low-power sleep mode" described on page 14 of the data sheet.
Here it is stated that entering Sleep mode when VCC is set to 0 V while voltage is being input to the BAT pin.
In addition, the description of "electrical characteristics over recommended operating free-air temperature range" in data sheet P4 also contradicts.
Here, the value of I (VCCS) when V (BAT) - VCC ≧ 0.8 V is described.
Which is right?
Thanks, Masami M.