I have a prototype board with bq26420. The battery charge circuit seems to working fine - detects when the voltage falls low, and then recharges the battery with the correct current. However the /PG and STATUS outputs are not working correctly.
The board is powered by a bench power supply. The 24V DC in is clean and stable, but the /PG output (used to drive an LED to +24V via 2k2) turns on for about half a second at power up, and then starts switching on and off - on for about 15mS, off for 30mS. The STATUS output (also an LED to +24V) is always off - even when the chip is recharging the battery (actually a bank of capacitors, 40000uF that I use for test purposes).
Do you have any ideas as to what might cause this? I checked my circuit and don't see any other signs of instability or bad connections.
thanks in advance
Daniel