This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2951 Single Cell Battery Charger

Other Parts Discussed in Thread: LP2951

Hi all, I am rather new to TINA and I have been trying to simulate the reference circuit shown in a Battery Charger with the use of a LP2951 for some low power solar cells project that I am working on. The problem I encountered is that it does not show a negative voltage when it should be around 5V at the output of LP2951.

I tried following the datasheet as it says that the Vtap and Sense pins should be open, but it does not say anything about the Error pin (tried connecting it to Vout and still the voltage is negative).

Vin = 6V, Vout after diode drop and adjusting the Pot should be under 4.2V. 

I would like to build one and test it out if this simulation is successful. 

Thank you.