I ordered a Gauge Development Kit to test a battery pack with a bq27411-g1.
Using the recommended setup, I am able to charge the battery pack properly. The current set is close to the current measured by the gauge. However, when discharging, I only get a fraction of the current that is set. For example, if I set 2000mA of discharge current, I get 267mA from the gas gauge and an amp meter.
Is is necessary to update the GDK firmware, as I have not been able to download the firmware update from the TI site yet.