Other Parts Discussed in Thread: TPS650830EVM-095, USB2ANY, TPS650830, TPS65185EVM, TPS650941EVM-116, TPS650860EVM-116, TPS65185, IPG-UI, LM75A
Hi,
My customer perchases TPS650830EVM.
Is "TPS650830EVM-095" include USB2ANY?
Bestregards,
Shimizu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS650830EVM-095, USB2ANY, TPS650830, TPS65185EVM, TPS650941EVM-116, TPS650860EVM-116, TPS65185, IPG-UI, LM75A
Hi,
My customer perchases TPS650830EVM.
Is "TPS650830EVM-095" include USB2ANY?
Bestregards,
Shimizu
Hi Shimizu-san,
I do not believe so. There is no indication that this will ship with a USB2ANY.
Update (12/15/2016): The TPS650830 EVMs now ship with a USB2ANY included in the kit.
Best Regards,
Rick S.
Hi Matsuro-san,
The GUI needs the USB2ANY to operate, and it does not appear to be bundled with the EVM a USB2ANY is included in the TPS650830EVM-095 kit.
You might need to acquire one internally for your customer if they intend to use the GUI, otherwise they can directly interface with the i2c pins using TP110 and TP111 and a generic I2C host.
Best Regards,
Rick S.
Hi Rick,
Thank you very much for the information.
By the way, do you have any idea of How we can buy USB2ANY?
Because of TI Store does not show the USB2ANY, we need to get it separatly.
Recently Power Management EVM like TPS650830EVM, TPS65094xEVM, TPS65185EVM, etc
these EVMs use GUI for USB2ANY but not USB to GPIO.
Please advice me,
matsuro
Hi Matsuro,
The USB2ANY cannot be ordered externally, but can still be acquired within TI.
The TPS650941EVM-116 does not need an external USB2ANY as it has one embedded on the EVM. Same with the TPS650860EVM-116.
The TPS65185 does not require a USB2ANY, as it ships with a USB-to-GPIO that works with the GUI on the product folder.
Most parts that ship with a USB-to-GPIO have a standalone GUI, but these GUIs are often platform specific. The USB2ANY is required if users want to utilize the IPG-UI, which is a cross platform universal GUI that can be used with multiple PMICs.
Best Regards,
Rick S.
Dear Rick,
How to purchase USB2ANY ?
TQ!.
Best Regards,
Patrick
+6012-4869099
Electromags Trading Sdn Bhd
25, Lebuh Rambai 12,
Paya Terubong,
11060 Penang,
Malaysia.
Hi Patrick,
The USB2ANY cannot be ordered, and would have to be requested through your local TI sales office.
Hi Patrick,
Generally speaking, the USB2ANY should come included with any kit that requires it. As an example, you could purchase the LM75A EVM www.ti.com/.../lm75aevm, which comes with a USB2ANY in the box.
Hi Rick,
Thank you for your update!
It is very helpful for customer.
Best regards,
Shimizu