Hi everybody,
I'm using a TFT screen from winstar. To control the backlight, I'd like to use the TPS61169.
Backlight's LEDs are made as follow :
9 lines of 3 LEDs. The global is current is 180mA (20mA per lines).
Rset = 240mV/0.18 = 1,13R
The TPS61169 will be supplied with 3V3.
On the other side, I don't understand how is provided/calculated Vout. In the datasheet, Vout is specified from Vin to 38V. Is Vout determined automatically according to the number of LEDs which must be supplied ?
Thank you,
Regards
Fabrice Péden