Hello,
I'm designing a product with 1S LiFePO4 battery / 1400mAh.
BQ34Z100 seems to be a good product, because i need to return SOC to the user with LEDs.
But I'm a bit disturbed by the current and the fact that the gauge seems to be always connected to the battery...
My product will have 90% of is life without be used, so if I let my pack connected to the gauge (even in sleep mode=84µA) I will lost about 4.3% capacity per month and about 50% per year. What is quite big... and lose interest of lithium benefit (less self-discharge). Deep sleep is better but still 18% per year.
Is it possible to connect the battery to the BQ34Z100 only when I need it (charging and discharging)?
Is there another way to deal with this problem ?
Regards,
Hubert