Hello Team
My customer VVDN is making an Access point
He is using POE PSE controller from TI tps23861
I have a few queries on the same
We are using the quad port PSE Controller "TPS23861" as suggested by you. We find a reference design "TIDA-00290" based on the same on TI website. We have some doubts regarding that design.
It has two modes of operation:
1. "Auto Mode" in which all the micro processor/controller pins "SCL, SDAI, SDAO, SHTDWN, RESET, INT & A3 are not used.
2. "Semi Auto Mode" in which it can be controlled by the host processor using I2C & other interface signals.
I want to know the functionality of "SHTDWN" pin in detail. Can we left it unconnected in "Semi Auto Mode",or we need to tie it to VDD or is it necessary to interface this pin with the host processor. What will be the consequences in each case. Please describe in detail.
Similarly please help me understand the same for Pin "A3"
I understand it will be used in case of multiple PSE controller ,
But in my case I have used only 1 port and only 1PSE controller in the entire system ,
So I believe even the SHTDWN pin need not be handled
Also in the TIDA-00290
In the mother board schematic
please help me understand why the buffer is used rather than just a Simple short
what relation does this SDA and SDAO have with isolation
I mean if we are making an isolated system is it necessary to have a 3wire i2C communication between uC and PSE
What is PSE_SDAO for ?