Other Parts Discussed in Thread: TPS61040, LM2577, LM27313, TPS61046
I was using LM2577 to boost a 3.6V battery voltage to 8.0V to power a sensor board. It was working just fine but has it's own issues since LM2577 is pretty old and has a big footprint and external components and is expensive and I don't need that much output current so I decided to use TPS61040 instead. First It looked like what I wanted with 400mA swtich current and everything cause I just needed 50mA output current but turns out it is 400mA SWITCH current NOT the actual OUTPUT current and apparently they are different!
It's a shame I didn't know that and never noticed that. By the way if anybody can clear this for me I would really appreciate that. How there two currents are different from each other and how was I supposed to know the output current? There should be some sort of an equation I think.
Now the output voltage decreases from 8.0V after connecting the sensor board to the output and I blame output current cause once I increase the input voltage from 3.6V to 6.0V it works fine.
So after wasting my time and money I'm looking for a better substitute for LM2577 and my requirements are:
Vin(max) = 3.6V
Vout(max) = 7.5V ~ 8.0V
Iout(min) = 50mA
Iout(max) = 80mA
I want it to have a small footprint and few external component requirements. (oh and no shocking price!)
Does anybody have an idea?
Edit: Considering the fact that this is a battery powered device it is better to draw less power from the input terminal while the converter is ON. (It's working only for a minute or two in entire day)