Hi guys and girls,
I'm trying to create a project with 4 servo's but the peak current of the individual servo's can get 8A or more.
Now i would like to do it with a single SMPS to convert the input voltage from a 4c lipo battery to 6V with a peak current of 4*8A + 25% = 40A
I couldn't find any circuit that could realize the following specs:
input: 12,8-16,8V
output: 6V 40A
The cooling is not really a problem because it going in a case that is submerged in water.
tnx for the help