I'm using the LM25069-2 Hot Swap Controller to supply 12V to our CPU board which typical draws 6 amps. The current limit is set to ~40amps and we've seen no issues with start-up until we've added the ability of the board to also provide the switched 12V to an external fan. The fan is rated at a max current of 1.2amps. The board fails to start with the fan connected. Looking at the fan current waveform when the switched 12V is supplied I don't see the fans initial start-up current exceeding 2.5 amps and the shutdown occurs well before the LM25069 fault timeout period. Has anyone experienced a similar issue when driving a DC fan . Any insight would be appreciated.
Thanks