Hi everyone,
We are working on a project and using your reference design one which is PMP9649. Input voltge range is from 85V to 265V and output current is 400mA in the reference design. However, we want the input voltage range to be around from 50V to 150V and its output voltage also should be 48V/1A or 12V/4A. Is it posibble for me to use the input voltage range or the output voltage / current at level which I have mentioned you ? Or is it better for me to use your another option which you can suggest ?
P.S: We don't want to use a transformator in our design. Because it is custom and too expensive.
Best Regards.