Hi, I have a few queries regarding the permanent fail and deep discharge of cell.
1) Suppose the device enters into Permanent fail, how to get out of it if I dont have any communication interface with the IC ? Any automatic reattempt is possible?
2) Consider a situation where the discharge FET's drain to source gets short and load is connected. Won't the battery deep discharge, as there is no other provision to disconnect the load from the battery?
3) Consider situation number 2 happens and the battery got deep discharged. Now I will have to replace my circuitry, to correct the Drain-Source short. Now the battery is at a very low voltage, say less than 2 V. Can I just change the circuit and connect the same battery? Or should I take it out and charge it separately to 2.5V and then connect back to the new circuit ? Or will the battery become altogether useless?