Hi
My customer will use LM3409HV under conditions.
When they use it in worst case, the duty cycle is 100%.
Could you tell me this devise's max duty cycle?
LED
・Vin:60V(ripple is ±5V)
・VF:typ55V
・IF:360mA
・Fsw:150~200kHz
Best regards
Yokota