This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about TPS61170

Other Parts Discussed in Thread: TPS61170

Hi,

Is the following condition possible with TPS 61170?

specification
VIN: 9 V
VOUT: 9.5 V
IOUT: 0.2 A

I think that it is necessary to consider min on time, but only the typ value is described.

Best Regards,

  • Hi,

    TPS61170 can be used in this applicaiton. You needn't worried about the minimum ontime. it will enter into the PFM mode and the output voltage will always 9.5V.

    Could you please share the detailed application information for us? Like in what kind of equipment? Volume? MP schedule? This is also oen of our work :) You can send the information to me by email, my email address is helen-chen@ti.com.