This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08T250W simple questions

Other Parts Discussed in Thread: PTH08T250W

Hello,

I'd like to use TI's PTH08T250W for our network switch application, and have several questions as below.

1. Can I use two PTH08T250W parts for Core voltage of 100A application?

2. If answer of 1st question is yes, how can I design peripheral interface circuit (include CAP or others if needed)?

- for check and prepare the space for PTH08T250W.

3. I cannot find the EVM or reference circuit for PTH08T250W. Can you share something that I refer to?

  • TS Yang:

    PTH08T250W current sharing information is located in the product specification starting on page 27..

    1. The ambient temperature vs output current limit  thermal data for (2) current sharing  PTH08T250W's is located  on page 26. Thermal data with 200 LFM air flow   air circulating fan, and 60 °C ambient  operating temperature, maximum output current is 90 amps.

    Contact me directly at tguerin@ti.com  if there are any other questions . I can also send your e-mail to the local TI technical group in your area.

    Tom