This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54295 and TPS54528 - VREG5 when Vin is less than 5V

Other Parts Discussed in Thread: TPS54295, TPS54528

Hi all

Would you mind if we ask TPS54295 and TPS54528?
How much is VREG5 when Vin is less than 5V? Will it be 5V?
(VREG5 is typ 5.5V in case of 6 V < VIN < 18 V)

We need your help always.

Kind regards,

Hirotaka Matsumoto