Other Parts Discussed in Thread: TPS54426, TPS62095
I'm seeking feedback regarding the TPS62095 vs the TPS54426, both 4A buck regulators.
I have used the TPS54426 before, and I was just testing it on the lab bench again. I get solid efficiency numbers ( high 80's ) and very low ripple on the output, which is great. However, I'm a little concerned that when I punch in numbers for a 4A buck regulator in the TI "Power Quick Search" box, the 54426 doesn't come up.
The top choice is the 62095, and I see that it has better efficiency numbers. Looks like the BOM cost would be close.
It also looks like the 62095 is a much newer part. And, I see that there is a family of these DCS parts just like there was with the DCAP-2.
Is it now an obvious choice to use the 62095 (DCS) over the 54426 (DCAP-2) for a new design, or does the former have some drawbacks? I see that it switches at about twice the frequency and accepts a lower Vin max, but that's OK. It's input would be a 5V wall wart.
Depending on the feedback I receive here, I think the next step will be to evaluate both of these on the lab bench for data such as ripple and switching / RF noise using near field probes.
Thanks
Bob