Hi,
I have a confounding problem with the LM5175 that I am hoping someone in the community can help me with.
I started with the LM5175 demo board. For my application (Vin = 10V-28V, Vout = 24V) I used WebBench to identify the recommended components. Assembled these components onto the demo board. Everything looked stable across the input voltage range, up to 4A.
I then designed a board to incorporate this design (Rev. A). Everything looks just like it did on the demo board.
I had to spin the board (Rev. B), and as part of the redesign the power supply section had to be relocated, but is largely the same layout. Also, the redesign included a change in FET's to keep them cooler under max. load (from NXP PSMN011-60ML to CSD18531Q5A).
Rev. B is now assembled, and at 4A, with the LM5175 in buck-boost region (most specifically around 21V-22V) the 24V output has a ~700mV, ~50kHz oscillation (switching frequency is set to 394kHz) riding on top of 24V. Further, when sweeping from 22V to 19V the 24V output will occasionally apparently shut down, falling to 12V, before the power supply recovers.
Anyone have any thoughts on what could be causing this Rev. B behavior? I have tried green wires, part replacement, and additional caps everywhere I can see/think where the problem may lie. I am about to the point of hand assembling the 24V power supply from scratch on a bare PCB to see if the problem can be recreated (I have observed this issue on (3) machine assembled PCB's).