This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53915 / Tolerance of VOUT_ADJUSTMENT



Hi,

Please let me ask about tolerance of  VOUT_ADJUSTMENT. Is following my understanding correct?

  • In case of +9% adj with VDACTOL1(typ) : Vref = 600mV + 54mV = 654mV (+9%)
  • In case of +9% adj with VDACTOL1(min) : Vref = 600mV + 54mV - 4.8mV = 649.2mV (+8.2%)
  • In case of +9% adj with VDACTOL1(max) : Vref = 600mV + 54mV + 4.8mV = 658.8mV (+9.8%)

Best Regards,

Sonoki / Japan Disty