This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EM1401EVM Baudrate Change

I am following the instructions below to set up the EM1401EVM. I have administrative abilities on the computer, but I still cannot change the baudrate to the required 500 Kbps. I have had IT change the administrative settings, but when I use the prompt below the says it cannot make the change. Is there any other way to set up and run the device.

To set the baudrate required for operation at 500Kbps you must call the script "regmodify.vbs" with the desired COM port at the Windows command prompt, in the path of the driver files (USB-CAN\Driver) like this:
"cscript regmodify.vbs COM15"