This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53647 / parallel configuration

Guru 29720 points
Other Parts Discussed in Thread: TPS53647

Hi Team,

Is it possible to operate in a parallel configuration of some TPS53647s with current sharing?
If the answer is yes, my customer considers to use TPS53647 for the following specification.
---------------------------------
Input voltage: 10~14V
output voltage: 1V
output current: 200A
---------------------------------

Best Regards,
Yaita / Japan disty