Other Parts Discussed in Thread: TPS56221
Dear TI engineer,
Dear All,
We produce radar signal board, based on C6000 DSP platform, the power supply chip is DCDC buck converter TPS56221.
When our products worked over a period of time(about two years),quite a number of the products malfunctions.
The malfunction appears that after a specific section of code is executed on the C6000 DSP,the electric current largen(about 10A) and the voltage fluctuates(about ±100mV) and then the C6000 DSP crashes.
normally,the C6000 DSP and the board will consume more cureent(about 10A) than usual when the section of code is executed ,but the voltage do not fluctuatesand and the C6000 DSP do not crashes.
A temporary solution :replace the TPS56221 on PCB for a new one.
What is the cause of this,please?
What should I do?
Thank very much!