Hi Team,
One of our customer is designing boost converter for below spec for automotive application and we suggested LM5121-Q1, LM5022-Q1 and TPS40210-Q1 for the application, but for all the devices the max output current is shown less than 20A in ESP, what to know what is the limiting factor for output current. LM5121-Q1 is more suitable for customer application as the device is having other additional features needed for the design. Even if these device is having enough gate drive current please let know what is the limiting factor for output current of 40A.
Input : 6V to 36V (with load dump protection upto 54V)
Output : 48V 30A
Thanks in advance for your support.
With Regards,
Shinu Mathew.