Hi,
Can the DCP010505BP dual output version be used to generate a +5V and -5V output simultaneously? It looks like it can, but I would like to confirm.
Thank You,
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can the DCP010505BP dual output version be used to generate a +5V and -5V output simultaneously? It looks like it can, but I would like to confirm.
Thank You,
Mike
Mike:
DCP010505DBP is an ±5 isolated unregulated converter . At 75% load on each output , 75mA , the output voltage range is ±4.25V minimum , typical is ±5V, maximum ±5.75V with input voltage of 5V ±1%. .
Tom