Hi Team,
Does the TPS544B25 support spread spectrum through an external clock? Our customer would like to vary the frequency between 850kHz-1.125MHz in order to reduce EMI (feel free to email me for specifics). If not, do we have a device that supports this and meets the following requirements?:
Vin: 12V
Vout: 5.5V (min)
Iout: 15A (max)
Vout ripple: <3mVpp
Total area: 500mm^2
The ripple spec seems very aggressive for 5.5V, so feel free to comment on what can be expected from this device.
Thanks,
Antonio