This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563200 OCP

Other Parts Discussed in Thread: TPS563200

Dear Sir,

What is the OCP value when the output voltage is 5V for TPS563200?  

Thanks, Ian.

  • Hi Ian,

    The current limit level shown on the datasheet is based on the ATE temperature char result. It is tested under test mode and the value is indicating the valley inductor current limit threshold. This valley current limit threshold is identical for different working condition including 5Vout. Please keep in mind that the average output current is one half inductor ripple higher than the valley inductor current.

    Best,

    Anthony