This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High power solution

Other Parts Discussed in Thread: LM5175

Hi all.

I would like to know the following high power solutions.

・Case 1
Vin=10V~60V
Vout=19V
Iout=14A(max)

・Case 2
Vin=8V~48V
Vout=19V
Iout=14A(max)

I think the solution can not be realized by nom-isolated DC/DC because of about 400W.
So please tell me the device that can realize and circuit constitution.

Best Regards,
Sho