Hi, I am looking to use the BQ24070 to run a GSM application from VOUT and also charge a 10.2Ah battery @ 1A as a backup supply. I am using the TI eval board for investigation.
If charging a flat battery, the maximum charge time of ~10hours may not be sufficient for full termination, so I disabled the timer by connecting TMR to VREF via 1k resistor. The datasheet (page 7, note 9) states that connecting TMR to VREF will disable the safety timer and charge termination. I presume that charge termination still occurs when the charge current has reduced to ISET/10, but it is the indication of charge termination that no longer works. Please confirm.
My battery appears to charge OK, but I do not see charge termination indicated by STAT1 and STAT2 change of state.
Thanks.