Hi,
Is it legal to tie OUT1 and OUT2 together on the TPS2561 as well as EN1 and EN2 together and FAULT1 and FAULT2 together? If I do so, do I set the ILIM resistor to be half of the output current? For example, if I set ILIM resistor to be 500mA, the FAULT will trigger when OUT reaches 1A (which is OUT1 and OUT2 tie together) ?
Thanks,
Luc