This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22990 QOD RESISTOR

Other Parts Discussed in Thread: TPS22990

E2e,

Does the QOD resistor in the TPS22990 have a maximum wattage specification?

Thanks for your help!

Regards,

WH

  • Hi WH,

    The maximum wattage for the resistance is derived from the maximum voltage for the device (6V) and the QOD resistance (218Ω). When the switch is turned off under these conditions, 6V is put across the resistance and 27.5mA is discharged through the resistance. At this point, the total power dissipated across the QOD resistor is 147mW, and the resistor is rated to handle this power.

    If the concern is the amount of time the resistor is dissipating power, then that is due to the capacitance on the output. However, this device is meant to handle capacitances even greater than 100uF with no issue.

    Thanks,

    Alek Kaknevicius