This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2000: BQ2000 Charging from USB

Part Number: BQ2000

Dear All,

I am planning to use BQ2000 as a charge controller IC to charge three standard rechargeable NiMh AA cell having nominal operating voltage of 1.2V. I would be charging the IC with the USB having 5V and 500mA.

Kindly provide your valuable feedback for the following : 

  1. I read in the TI document that BQ2000T should be prefered as compared to BQ2000 due to its full charging termination method. Kindly suggest me which charge controller IC should be used. I have hereby attached the technical document for your reference.
  2. As per our applications, we would be charging three standard AA cell  with the USB having 5V and 500mA. Would it be suitable to charge three standard AA cell with BQ2000?

Looking forward for your prompt response

Thanks & Regards,

TANVI GUPTA