Hi,
I am planning to use LP38693MPX-1.8/NOPB to generate 1.8V from 3.3V. Could you please share the design for the same?
Thanks,
Regards,
Meria Jacob
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am planning to use LP38693MPX-1.8/NOPB to generate 1.8V from 3.3V. Could you please share the design for the same?
Thanks,
Regards,
Meria Jacob
Hi Meria,
Your circuit looks good. One thing what I see is input and output capacitors capacitance value. I see you have specified them to be 16V tolerating 1uF capacitors so capacitance derating due to dc voltage bias will be quite small but temperature also affects. So recommended is to use good temperature coefficient capacitors (temperature types Z5U, Y5V or X7R/X5R) or increasing value to 2.2uF.
Best regards,
Jari Niemelä
Hi,
We are using the following capacitor for C2 and C4
CC0603KRX5R7BB105 | CAP CER, 1UF, 16V, X5R, 10%, 0603 | YAGEO |
For C3 we are using
C0402C104K4RACTU | CAP CER 0.1UF 16V 10% X7R 0402 | KEMET |
Could you please confirm if the part number LP38693MPX-1.8/NOPB and the value of R45 is correct?
ERJ2RKF4703X | 470 Kohm, 100 mW, ± 1%, 50 V | Panasonic |
Thanks,
Regards,
Meria Jacob
Hi,
Per datasheet capacitors are as recommended. LP38693MPX-1.8/NOPB is SOT-223 package version. R45 value is quite high it could be a lower value also since EN pin has high input resistance itself. If EN pin is not needed it should be tied straight to the VIN voltage ( actually datasheet claims straight connection to the VIN if EN functionality is not needed).
Best regards,
Jari Niemelä