Other Parts Discussed in Thread: UCC28180
I'm currently trying to implement a PFC solution based on the UCC28019. I have the UCC28019EVM unit and I'm being tripped up by the magnetics.
The EVM BOM calls out a 1.25mH inductor. The inductor on the board is physically HUGE. (2.5 inch diameter torroid, about 1 inch thick) I ordered some 2 and 4 mH inductors from my usual sources and they are much smaller (one inch largest dimension).
I've done a few tests on the EVM with moderate load (operates as expected), significant overload (surprisingly well behaved).
Now I've swapped the inductor for one of my off-the-shelf units (DENO-25-0001) and attempted to test the (now modified) EVM again. It will not hold output voltage with even half rated load.
So, I'm confused. Either one of these datasheets is lying to me about the size of the inductor, or there's another factor I'm missing somewhere. I'd appreciate a bit of guidance. My suspicion is that there's something about the ferrite composition of the supplied inductor, but I cannot find a proper datasheet for it, so...
This is for a very low volume product (less than 50 pcs/yr) so stock magnetics are greatly preferable.
Thanks