I used BQ2057WSN with FZT788B or SI6475DQ to charge 2 cell li-battery.the Vin 9V Rsns 0.1Ω. I test the charge current about 1.2A.but the FZT788B or SI6475DQ are very hot. how can I solve this issue. can you advise a p-mos to me.thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I used BQ2057WSN with FZT788B or SI6475DQ to charge 2 cell li-battery.the Vin 9V Rsns 0.1Ω. I test the charge current about 1.2A.but the FZT788B or SI6475DQ are very hot. how can I solve this issue. can you advise a p-mos to me.thanks.
Hello,
You are going to encounter similar issues regardless of what PMOS device you choose. The reason being that the PMOS device is the in-line regulating element for this linear charger. This means that if you battery voltage is down at 6V and you are charging at 1.2A from a 9V source there will be 3V across the PMOS device at a current of 1.2A meaning that it is dissipating 3.6W and as a result will get very hot.
Have you considered using a switch-mode battery charger? This will be far more efficient and therefore not get nearly as hot.