Hi
The company where I work have a project that use the UCC29002 and we are having problems with the LS signal: when we measure this signal in different boards with the same load, the signal is different. The output signal to load is same between boards. I would like to know how this signal LS should be and if exists some simulation tool for this component?
Output signal load: 5,2V
Current load: 3A