Hello there!
I'm designing a backup power system with boost converter that'll supply 3.3/5V from LiPo Battery. I'm using TPS63020 as BuckBoost Converter and TPS22910 as a switch. Here's what I'd like this device to do.
1. When USB is connected, TPS22910 will stop working. So, 5V will either be bought down to 3V3 or will be outputted according to Jumper (J1) selection.
2. When USB is disconnected, TPS22910 will turn on. So, LiPo Voltage will enter 63020. Output of regulator is dependent on Jumper(J1) selection.
I drew the schematic and need your help in verifying the same. Specifically, the following points:
1. In my design, user can select the output to be either 3V3 or 5V depending on jumper(J1) setting, Setting J1 to left will set the output to be 3V3 while setting it to right sets the output to 5V. I calculated resistances using R1 = R2(2Vout - 1) formula(Vref = 0.5V) as mentioned in DS. Can I change the output by selecting FB resistors through jumper?
2. I'd like user to have full control over converter. So, am exposing PS/SYNC and EN pins. Did I draw both connections correctly? Are PullDown on PS/SYNC pin(10k) and Pullup resistor(10K) on EN pin fine?
3. Did I connect PGOOD pin correctly?
Other than these three, is everything in schema looking good? Please let me know.
Teja