This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43602-Q1: Output Capacitor Selection

Part Number: LM43602-Q1

Hello,

Would you let me know how the equality 19 and 20 in the datasheet shown below were derived?

Or make a brief explanation about what is compared to what in these inequalities?

One of my customers is making a lot of trouble to understand it.

Thank you.

Oguri (TIJ automotive FAE)

  • Hello Masatoshi-san,

    I moved this post to the SIMPLE SWITCHER forum and will forward the question to the applications engineer for this device.

    Regards,
    Denislav
  • Hello,

    One of the purpose of the output capacitor is to hold up the output voltage when there is the load experiences a surge. Customers will have different specs on what the max droop they wan to allow. The capacitor needs to be sized according to that. The components of the equation are 

    r = ripple ratio.
    deltaVOUT = allowed droop

    What the equation says is that if you choose a capacitor value higher than calculated, you should be able to obtain the load surge response you wanted. This doesn't completely factor in the internal loop compensation. I have attached a presentation that details the calculation.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/Capacitors-Calculation-for-DC_2D00_DC-Converters.pptm