Hello
I am doing a design where the backplane voltage is -48V, output is 12v at about 4Amps. Does TI have a part for that?
Also why use -48V? Does it have to do with relability of the connections?
Thanks
Timothy Darling
Designer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Timothy
Is the input voltage -48 constant, and do you need isolation for this power you are going to design?
If isolate is needed, LM5021 is my recommendation.
If isolate is not needed, you should post your question on below forum.
https://e2e.ti.com/support/power_management/non-isolated_dcdc/
-48 connection, means positive port connect to ground. This connection is going to protect power supply from damage.
Regards,
Yunsheng
Hi Timothy,
I encourage you to use the TI Reference Designs page: http://www.ti.com/general/docs/refdesignsearchresults.tsp
I used -48V Min Input, 12V Min Output, no value in Output current, and a close design is the 125W Inverting Buck-Boost using the LM5122:
125W Inverting Buck Boost for Telecom Power Amplifier Reference Design . This PMP20371 would be a good starting place for your design, you can modify it for your requirements.
~Leonard