I am designing a Power Conversion small circuit card using the LM2941LD part. The estimated maximum output current is 0.225 amps with an input voltage of 15-19 V DC. I have selected Resistor values for R1 = 1 K and R2 = 10 K for an output of approximately 14 V. The maximum operating temperature is 55 Deg C.
1) For Cin, I have tentatively selected a 0805, X5R, 35 V 0.47 uF, 10%.
a. Is this style(X5R), value and DC rating appropriate for my circuit application? Yes, I will place Cin as close to the LM2941 as possible - same side as LDO.
2) For Cout, I have tentatively selected a 1206, X5R, 25 V, 22 uF, 10%.
a. Is this style (X5R), value and DC rating appropriate for my circuit application ? I will be operating Cout at approx 14 V (56% of 25V rating)
b. Should I also include a series resistor ? How do I calculate value and wattage ?
For this design, the physical space is limited so I do not have room for a large size tantalum output cap.
Thanks for any design assistance.
Best Regards, Gary